Case Studies
The modernization of operational technology (OT) systems in addition to the increased automation of industrial control systems (ICS) have created an explosion of network-connected equipment. This can expose industries and their critical infrastructure to a wide range of cyber threats from nation states, criminals, disgruntled employees, and accidental misconfigurations. Further, OT networks and ICS were physically separated from traditional IT infrastructure are increasingly interconnected, creating unique security issues.
Ransomware, extortion, and financially motivated cybercrimes top the list of threat vectors that concern industrial cybersecurity teams. A successful ransomware attack, for instance, can be damaging to an organization on multiple fronts: the attack can interfere with and disrupt command and control of critical data and infrastructure, and attackers typically demand millions of dollars from the victim in exchange for restoring access to data and/or operations.
There has never been a more pressing need for industrial cybersecurity teams to monitor and protect their organization’s critical infrastructure and systems.
Situation and Key Objectives
With over twenty mining, metallurgical, and chemical plants across Mexico, this large industrial operator has a significant OT infrastructure that needs to be monitored and protected. In response to expanding threat vectors and rising threats, the customer launched a company-wide cybersecurity program that looks to strengthen internal cybersecurity capabilities, with the goal of reducing cybersecurity risks. The program initiatives can be mapped to the NIST Cyber Security Framework and grouped under four elements: Prevention (opportunities for cybersecurity improvement and strengthening), Detection (continuous monitoring and cybersecurity vulnerability management), Identification (e.g., asset inventory, etc.) and Remediation (e.g., corrective actions planning).
As part of Prevention, Detection and Identification initiatives, the company’s OT security team procured a sensor-based OT security solution that combines behavior-based anomaly detection with signature-based threat detection. The company initially tried to leverage SPAN ports to supply OT security sensors with packet streams, but quickly ran into several limitations:
• OT security sensors not having enough ports to ingest all the mirrored traffic. While the customer had the option to deploy additional OT security sensors, i.e., more ports, inserting a visibility platform was a more flexible, simpler, and cost-effective option.
• Some legacy switches were incapable of mirroring traffic.
Keysight was selected to provide enhanced network visibility and to ensure the OT security sensors received all the relevant traffic - no blind spots. The Keysight visibility team collaborated extensively with the firm’s OT security team, and the OT security solution vendor, on a visibility design that addressed existing blind spots, while also ensuring flexibility for future visibility needs.
The Visibility Solution
Flex TAPs were deployed to access traffic from optical links across various locations. Keysight Flex Tap passive fiber optical TAPs provided an exact copy of network traffic, without impacting equipment on the network, ensuring a seamless, reliable capture of traffic.
Keysight Vision NPBs (network packet brokers) were deployed at each of the company’s plant locations. Positioned between the traffic acquisition points and the OT security sensors, the Vision packet brokers function as a packet distribution layer, aggregating, replicating, and redirecting the acquired traffic to the different OT sensors.
×
*Indicates required field
Thank you.
A sales representative will contact you soon.