N9083EM0D Multi-Standard Radio (MSR) X-Series Measurement App, Traditional UI

Technische Überblicke

Keysight Technologies

N9083EM0D Multi-Standard Radio (MSR) X-Series Measurement App, Traditional UI

Technical Overview

– Perform MSR base station transmitter tests on any combination of LTEFDD,W-CDMA/HSPA/HSPA+, GSM/EDGE/EDGE Evolution, cdma2000, and 1xEV-DO signals

– Perform one-button tests per the 3GPP Release 10 standard (TR/TS 37 series)

– Use hardkey/softkey manual user interface or SCPI remote user interface

– Leverage built-in, context-sensitive

Multi-Standard Radio (MSR) Measurement Application

The MSR measurement application transforms the X-Series signal analyzers into standard-based MSR base station transmitter testers by adding fast onebutton RF conformance measurements to help you evaluate and manufacture your MSR base station and base station components.

X-Series measurement applications can help you:

– Gain more insight into device performance with intuitive display and graphs for your application. Select from our library of over 25 different measurement applications.

– Ensure that your design meets the latest standard. Updates are made to the X-Series measurement applications as standards evolve.

– Apply the same measurement science across multiple hardware platforms for consistent measurement results over your design cycle from R&D to production.

– Choose the license structure that meets your business needs. We provide a range of license types (node-locked, transportable, floating or USB portable) and license terms (perpetual or time-based).

Multi-Standard Radio (MSR) Technology Overview

The rapid evolution of mobile broadband and the need to deploy next generation cellular technologies alongside legacy deployment has lead to development of multistandard radio (MSR) base stations. 3GPP defines an MSR base station by the ability of its receiver and transmitter to process two or more carriers in common, active RF components simultaneously in a declared RF bandwidth, where at least one carrier is of a different radio access technology (RAT) than the other carrier(s).

The key drivers behind MSR are coexistence of different technologies in a single network, spectrum “refarming,” and cost reduction. MSR allows operators to put spectrum space to a new use, resulting in seamless network migration from the currently deployed 2/3G radio formats to 4G. In terms of cost reduction, using the same base station hardware for multiple technologies reduces the number of sites, site rental costs, and the amount of on-site equipment required.

Traditionally the RF specifications for base station transmitters and receivers have been developed separately for the different RATs. However, in an MSR base station, the base station transmitter and receiver is capable of simultaneously processing multiple carriers of different RATs using common RF hardware, requiring a new set of RF specifications. As such, 3GPP developed a dedicated RF specification for MSR-capable base stations in the 3GPP Release 9 and 10 (TR/TS 37 series).

The operating bands for which MSR base stations are defined are divided into three different band categories (BCs): BC1 for LTE-FDD and W-CDMA operation; BC2 for LTE-FDD, W-CDMA and GSM/EDGE operation; and BC3 for LTE-TDD and TD-SCDMA operation. MSR conformance tests are required when carriers of multiple RATs are being activated. This is done through a set of multi-RAT test configurations (TCs) of contiguous and noncontiguous frequency allocations. Required transmitter measurements in a multi-RAT configuration include channel power, modulation quality (EVM), frequency error, spurious emissions, and operating band unwanted emissions (SEM). Alternatively, ACLR occupied BW and time alignment between transmitter branches are performed in singleRAT configurations, as defined in the TS37.141 conformance requirements.