N9062A SCPI Command Language Compatibility X-Series Measurement Application

Technische Überblicke

Demo Guide

This document will guide you through the setup process for a Keysight Technologies, Inc. X-Series signal analyzer (PXA, MXA and EXA) with the SCPI language compatibility measurement application.

Compatible SCPI Commands

The SCPI language compatibility measurement application transforms the X-Series signal analyzers (PXA, MXA and EXA) into SCPI commands compatibility mode by supporting over 278 SCPI commands from R&S FSP/FSU/FSE spectrum analyzers.

This application enables the X-Series signal analyzers to understand the following SCPI commands from R&S FSP/FSU/FSE spectrum analyzers:

– General-purpose spectrum analysis settings: frequency, span, amplitude, RBW, VBW, sweep, detectors, trace averaging, data format and more

– General marker, delta marker, marker noise, band power, power density functions

– Limit line and limit check functions

– Limit check for spectrum emission measurements

– Power measurements: channel power, ACP

– Statistical measurement function: CCDF

– Trace data transfer and IQ data handling

– File saving and screen copy

What is SCPI?

SCPI is an ASCII-based instrument command language designed for test and measurement instruments, with the goal of reducing automatic test equipment (ATE) program development time.

SCPI accomplishes this goal by providing a consistent programming environment control and data usage. This consistent programming environment is achieved by using defined program messages, instrument responses, and data formats across all SCPI instruments.

By providing a consistent programming environment, replacing one SCPI instrument with another SCPI instrument in a system will generally require less effort than with non-SCPI instruments. SCPI is not a standard which completely provides for interchangeable instrumentation.

SCPI helps move toward interchangeability by defining instrument commands and responses, but not functionality, accuracy, resolution and other factors. 

Demonstration Preparation

This demonstration utilizes an X-Series signal analyzer with N9062A-2FP measurement application (F/W revision A.06.06 or greater). When N9062A-2FP is licensed, the SCPI language compatibility mode is available. 

The following software and accessories are used for demonstration in this document:

– Two LAN cables

– One PC with Keysight IO library suite (revision 15.1 or greater)

In the document, keystrokes surrounded by [ ] indicate frontpanel hardkeys; softkeys located on the right edge of the display are surrounded by { }.

Demonstration

Connect the X-Series signal analyzer and your PC to a LAN

In this demonstration guide, the Keysight IO library connection expert is used.

Enter the SCPI language compatibility measurement mode

There are two ways to access the SCPI language compatibility measurement mode.

Select compatibility model

There are two ways to select a compatible model.

Set the IDN response (optional)

IDN response allows you to set or query the Mode IDN Response type to: compatible model, system or user defined. For example, if you choose the IDN response as {system}, the query *IDN? returns the instrument information of your X-Series signal analyzer.

You can choose either front panel access or remote access to set the IDN response.