3070 Test Analysis Tools

Datenblätter.

With increased outsourcing, board designers and test developers are not just in different departments these days. They’re often in different companies. How do you make sure that a purchased test meets the quality and coverage requirements of a given design? How do you make sure you’re covering the right components? How do you avoid duplicating tests? How do test managers, test developers and production engineers get useful information to improve test effectiveness? How do you determine the type of test coverage you’re really getting? So many questions, one simple answer. Keysight i3070 test analysis tools, available at no cost on every Keysight i3070.

You’re Covered

Keysight test analysis tools provide crucial coverage information to test managers, board designers and production engineers. Information is provided graphically, so it’s easy to understand and evaluate. Stakeholders who need to understand what’s really going on at ICT can now get the information they need in a format they can use.

Coverage Analyst:

Summarize, Navigate, Evaluate Unlike tedious text-based reporting tools, Keysight i3070 Test Program Coverage Analyst is easy to use, comprehend, and navigate. This visual reporting tool uses data from Keysight’s Board Test Grader and other tools to report on the coverage being attained by the Keysight i3070. It does this using color coding and other visual clues to display coverage levels with clarity and precision. Test managers use Coverage Analyst as a summary tool to evaluate coverage levels, test approach, and details that account for the overall result. Test engineers use it to drill down to greater levels of detail, and investigate where test coverage is adequate versus where it needs to be improved.

Production managers and contract manufacturers use it to evaluate exactly how good their Keysight i3070 test really is. And all stakeholders can use Coverage Analyst to document and prove the coverage levels they’re really getting with the Keysight i3070. Coverage Analyst eliminates not only guesswork but also the tedium of poring through pages of text-based analysis. 

-HTML web-style pages using color-coding, fonts and graphics to display coverage levels visually for easy understanding.

– Hyperlink connections make it easy drill down for additional layers of detail on any pin or device.

– Integrated views provide a complete and detailed picture, incorporating data from Board Test Grader and other Keysight tools.

Keysight Coverage Tool:

Filter, View, Share

The Keysight Coverage Tool combines data from ICT and X-ray test in a single coverage report. Keysight Coverage Tool is the filter that turns this test data into actionable information: it allows you to select the test coverage information you want to see, display the data on-screen in an integrated format, and incorporate the results in a report that can be displayed, printed or e-mailed. Keysight Coverage Tool parses available ICT and X-ray coverage data and displays the results graphically, making it easy to evaluate how different test cells are performing. You can identify specific components or leads, and verify the coverage you’re getting with the Keysight i3070 or the 5DX. 

It helps avoid duplicate tests, and allows you to verify that unpowered tests are providing adequate coverage across all devices and packages before power is applied to the board. 

– Choose what you see and how you see it. Use a variety of predefined filters for different on-screen views. Pinpoint trouble spots, for example: highlight gaps in test coverage while suppressing data on devices on leads that are well covered. 

– Create custom HTML reports that can be saved, printed or e-mailed with a few menu clicks.

–Work in your favorite browser. Get coverage reports on the same workstation that’s handling test development.