Case Studies
This case study presents a contract manufacturer producing laptop motherboards for a renowned computer brand. The manufacturer faced challenges in testing 400 boards per shift across two daily shifts and needed a solution to improve test speed, coverage, and flexibility. By putting the Keysight i3070 Series 7i ICT system to the test, the manufacturer evaluated its capability to meet their testing needs and identify potential enhancements. The evaluation demonstrated a 30% reduction in test time and an 11% increase in test coverage, showcasing the system's potential to enhance production efficiency.
Können wir Ihnen behilflich sein?