Datenblätter.
5G deployments will enable enhanced mobile broadband services with higher data rates, increased capacity, and lower latencies. New business opportunities and increased revenue sources can be found with Network Slicing, Mobile Edge Computing and Private 5G via massive and critical IoT services in sectors like automotive, manufacturing, energy and utilities.
But to ensure the carrier-grade quality required to carry this amount of wireless traffic, service providers need to characterize and continuously validate their 5G Core (5GC) network in the lab and pre-production deployments. This requires extensive testing of 5G SA (Standalone) elements in the Core network.
Challenges include:
Pre-Deployment Validation Using Real-World Subscriber Simulation
Keysight's 5G LoadCore™ test solution addresses critical validation requirements for improved reliability and performance of 5G emerging architectures. With comprehensive performance testing of all nodes and interfaces, this powerful yet easy-to-use solution helps network operators deliver higher-performing services, greater scale, and lower-latency communications.
Using real-world subscriber modeling, testers do not need to be protocol experts to develop realistic test scenarios. From a single application, perform capacity tests, detail a device’s throughput, measure voice and video quality, and model a wide variety of mobility scenarios.
With 5G development and adoption progressing rapidly, cloud native is central to the 5GC architecture. With its microservice architecture and options to be deployed either as a virtual machine (VM) or Container, LoadCore is fully aligned to this new paradigm.
Highlights
5G Core Network Validation
LoadCore is a comprehensive solution for the complete validation of the 5G Core Network. From end-toend to node isolation, LoadCore simultaneously simulates multiple nodes and interfaces, allowing the recreation of entire networks in lab environment by using a topology-based user interface (web UI).
The entire core is simulated, with each node independently deployed. User equipment (UE) actions (Registration/PDU Session Establishment/Modification, Handovers, etc.) are simulated across all 5G core nodes and interfaces, offering a complete end-to-end view. 4G, 5G NSA (non-standalone) and 4G/5G iRAT procedures can also be simulated for complete validation across multiple domains.
Können wir Ihnen behilflich sein?