Ruby Net FTP Command Injection

Strike ID:
E17-3i591
CVSS:
8.8 CVSS:3.0/AV:N/AC:L/PR:N/UI:R/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
5
Year:
2017

Description

This strike exploits a remote command injection vulnerability in Ruby before 2.4.3. The vulnerability is due to ruby NEt::FTP, which will execute any command after the "|" pipe character in the localfile argument. This vulnerability could allow an unauthorized user to execute arbitrary code on the server.

CVE

References

Bid