E18-mauz2
CVSS:
7.5 CVSS:3.0/AV:N/AC:H/PR:N/UI:R/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
1
Year:
2018
Description
This strike exploits a vulnerability in Microsoft Edge. Specifically, the vulnerability exists in the Javascript Chakra engine. It is possible to craft Javascript in such a way that an object is passed to the InstanceOf method to dereference a pointer value of an assumed type, which can be changed causing type confusion to occur. This may lead to a denial of service condition in the browser, or potentially remote code execution.