Keysight recommends using the most current version, which includes the most up-to-date bug fixes and security patches available.
Release Date Version Version Description
2023-03-23 5.5.1.81 CCL licensing update for older Infiniium oscilloscope software and Infiniium Offline software on oscilloscopes or computers with the Windows 10 operating system.
Release Date Version
2023-03-23 5.5.1.81
Version Description
CCL licensing update for older Infiniium oscilloscope software and Infiniium Offline software on oscilloscopes or computers with the Windows 10 operating system.

When to Update

  • Install this update whenever using a version of Infiniium specified in the Prerequisites.
  • If you downgrade Infiniium to a version listed in the Prerequisites, this update should be performed.

How to Download

  • Click the "Download" button and save the zip file to a temporary folder on your Infiniium oscilloscope or host computer that runs the Infiniium Offline software. NOTE: This update requires the Windows 10 operating system.

How to Install

 

  1. Make sure the Infiniium software version you want to use is installed before installing the CCL licensing update.
  2. Make sure no Keysight application software is running when installing this update. This includes the Infiniium software and Infiniium compliance applications.
  3. Right-click the downloaded zip file and extract the files to the temporary folder.
  4. In the extracted files, right-click the "Install-Ccl-Upgrade.cmd" file or the "Install-Ccl-Upgrade.ps1" file and choose "Run as administrator" (or some other option for running with elevated priviledges). The cmd file will execute in a Command Prompt window run as administrator, or the ps1 file will execute in a PowerShell window run as administrator. These scripts perform the same actions, and either one can be used.
To verify the installation:
  1. In the Windows Control Panel, go to Programs and Features, and then Uninstall a Program.
  2. Verify the Keysight License Manager version is 5.5.1.81.
  3. Verify the Keysight License Service version is 5.5.1.81.
  4. Close the Control Panel.
  5. Verify that the Infiniium software application starts.

 

Licensing

  • Does Not Require a License

Installs on: PC / Instrument

Operating System

  • Windows 10

Prerequisites

  • Versions 10.00 through 11.40 of the Infiniium UXR-Series Real-Time Oscilloscopes Core Software
  • Versions 11.00 through 11.40 of the Infiniium MXR-Series Real-Time Oscilloscopes Core Software
  • Versions 11.06 through 11.40 of the Infiniium EXR-Series Real-Time Oscilloscopes Software
  • Versions 6.00 through 6.74.00002 of the Infiniium Oscilloscope Software for Infiniium Z-Series, V-Series, S-Series, 90000 X-Series, and 9000 Series real-time oscilloscopes (Windows 10 operating system only)
  • Versions 6.00 through 6.74.00002 (Windows 10 operating system only) and versions 10.20 through 11.40 of the Infiniium Offline Oscilloscope Analysis Software (D9010BSEO)

Supported Instruments

  • Infiniium UXR-Series Real-Time Oscilloscopes
  • Infiniium MXR-Series Real-Time Oscilloscopes
  • Infiniium EXR-Series Real-Time Oscilloscopes
  • Infiniium Z-Series, V-Series, S-Series, 90000 X-Series, and 9000 Series oscilloscopes with the Windows 10 operating system
  • D9010BSEO Infiniium Offline - Base Software running on a computer with the Windows 10 operating system
No previous versions available
SHOW MORE