ビデオ
GNSS and PNT performance depends on rigorous testing. But traditional GNSS testing has always forced a tradeoff between the richness of the real world and the control of simulation.
SimXTRACT eliminates that compromise. SimXTRACT converts real-world RF recordings into fully controllable, repeatable lab scenarios, bridging the gap between record & playback technology and simulation. Engineers can deconstruct complex GNSS signal environments, identifying code error, Doppler, and power levels, and SimXTRACT rebuilds them with precision. This is not simply playback. It is signal-level reconstruction that transforms field data into powerful PNT testing assets.
With SimXTRACT, recorded RF environments become editable and controllable simulation scenarios. Teams can identify root causes faster, reduce field campaigns, and accelerate R&D cycles. Instead of chasing issues in the field, engineers bring reality into the lab – with full control over every parameter.
SimXTRACT redefines what GNSS simulation and testing can achieve.
For more information about SimXTRACT, visit: https://www.keysight.com/us/en/product/PNT24001A/simxtract.html
何をお探しですか?