Improving Power Supply Efficiency – 5 Hints

Notas de Aplicação

Introduction

Manufacturers continue to be asked to do more with less. Increasing throughput can reduce the amount of equipment used in test and the physical constraints of a manufacturing site. An improved work flow will also reduce inventory costs. The Keysight Technologies, Inc. Advanced Power Supplies are designed to increase throughput while providing the highest level of protection to your device under test. Read all ten hints to learn more about improving test throughput.

 

Improve Throughput with Shorter Command Processing Time

Improving test throughput starts with using faster power supplies. Command processing time is a key parameter governing a power supply’s speed as it affects virtually all aspects of its use under automated control. Shorter command processing time can significantly increase throughput by taking seconds off of the test time. This is particularly true when the DUT needs to be tested at several output level settings and corresponding current or voltage measurements taken, which is frequently the case.