Multiple F5 BIG-IP products Directory Traversal

Strike ID:
E20-12z21
CVSS:
9.8 CVSS:3.1/AV:N/AC:L/PR:N/UI:N/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
3
Year:
2020

Description

This strike exploits a directory traversal vulnerability in multiple F5 BIG-IP products. The vulnerability is due to improper handling of user-supplied path in HTTP requests. A remote, unauthenticated attacker could exploit this by sending a maliciously crafted request to the server. A successful attack may result in arbitrary file read, write or remote code execution in the security context of ROOT.

CVE