E19-0r4j1
CVSS:
9.8 CVSS:3.0/AV:N/AC:L/PR:N/UI:N/S:U/C:H/I:H/A:H
False Positive:
t
Variants:
1
Year:
2019
Description
A heap overflow vulnerability exists in the 'dhcpcore.dll' component of Windows DHCP Client.
The vulnerability is triggered by two subsequent null bytes in a Domain Search DHCP Option within a DHCP Offer packet, followed by an arbitrary number of bytes, causing a zero-length buffer to be written, thus overwriting a invalid memory space.
By exploiting the vulnerability, an attacker may be able to execute arbitrary code with SYSTEM privileges.