Können wir Ihnen behilflich sein?
Keysight Enables Engineers to Verify, Debug CAN XL and Other Automotive Protocols
New protocol trigger and decode software simplifies development /troubleshooting of various CAN bus systems
SANTA ROSA, Calif. April 21, 2022
Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that delivers advanced design and validation solutions to help accelerate innovation to connect and secure the world, has released the industry's first oscilloscope-based automotive protocol trigger/decode solution (D9010AUTP) covering CAN XL (Controller Area Network eXtra Long) that enables engineers to verify and debug low-speed automotive serial bus protocols and simplify the development and troubleshooting of systems including CAN/CAN FD (Flexible Data Rate) and CAN XL.
CAN XL is the third-generation CAN standard in development by the CAN in Automation (CiA) group that improves the well-established CAN FD protocol with increased payload data and faster bit rate. The CAN XL data phase speed is specified to reach 10 Mbps or more, depending on the transceiver capabilities and physical layer components. CAN XL has two modes of operation – fast mode and SIC mode (or slow mode).
Keysight's automotive decoder software triggers and decodes the SIC mode signal in the arbitration phase, as well as the fast mode signal in the data phase, correctly. It also handles the CAN XL protocols implemented with the CAN HS/FD/SIC transceivers.
"In-vehicle networking technologies play a pivotal role in transmitting data fast and reliably from sensors to AI decision making units, as well as in-between safety relevant electronic control units and electronic systems within the car," said Thomas Goetzl, vice president and general manager for Keysight's automotive & energy solutions business unit. "The variety of automotive serial bus standards reflects the diverse needs and requirements of the automotive industry, and Keysight is excited to continue providing industry-first solution offerings that support additional capabilities and use cases."
Keysight's D9010AUTP software is compatible with Keysight's Infiniium oscilloscopes using software version 11.30 or higher for MXR/EXR/UXR models and version 6.72 or higher for other Infiniium scope models enabling users to:
- Set up the oscilloscope to show CAN, LIN, CAN-FD, CAN XL, FlexRay and SENT protocol decode in less than 30 seconds
- Gain access to a rich set of integrated protocol-level triggers
- Save time and eliminate errors by viewing packets at the protocol level
- Use time-correlated views to quickly troubleshoot serial protocol problems back to their timing or signal integrity root cause
Additional information about Keysight's Automotive Protocol Trigger and Decode software is available at the Keysight D9010AUTP data sheet.
About Keysight Technologies
Keysight delivers advanced design and validation solutions that help accelerate innovation to connect and secure the world. Keysight's dedication to speed and precision extends to software-driven insights and analytics that bring tomorrow's technology products to market faster across the development lifecycle, in design simulation, prototype validation, automated software testing, manufacturing analysis, and network performance optimization and visibility in enterprise, service provider and cloud environments. Our customers span the worldwide communications and industrial ecosystems, aerospace and defense, automotive, energy, semiconductor and general electronics markets. Keysight generated revenues of $4.9B in fiscal year 2021. For more information about Keysight Technologies (NYSE: KEYS), visit us at www.keysight.com.
# # #
Additional information about Keysight Technologies is available in the newsroom at https://www.keysight.com/go/news and on Facebook, LinkedIn, Twitter, and YouTube.
Keysight Contact:
Geri Lynne LaCombe, Americas/Europe
+1 303 662–4748
geri_lacombe@keysight.com
Fusako Dohi, Asia
+81 42 660–2162
fusako_dohi@keysight.com
Keysight’s D9010AUTP decodes the SIC mode and fast mode signal generated by CAN SIC XL transceiver
Need to contact Media Relations at Keysight?