Cross-platform testing validates that an application works correctly across the full range of devices, operating systems, browsers, and environments users access it from. AI-powered cross-platform testing replaces the historical requirement of separate scripts per platform with a single test approach that runs everywhere.
AI computer vision interacts with applications the way users do, eliminating dependence on platform-specific selectors or back-end APIs. Eggplant applies the same test logic across web, desktop, mobile, Citrix, VDI, and device farm environments from a single test definition.
Eggplant uses next-generation AI computer vision to test applications the way users see them, regardless of platform, technology stack, or source code access.
Computer vision identifies UI elements visually, the same way users do, eliminating dependence on selectors or platform-specific access.
The same test runs across mobile, web, desktop, mainframe, and packaged applications, with no platform-specific rewrites required.
Run tests in parallel across devices, browsers, and operating systems from a centralized platform, scaling coverage without scaling effort.
Manage, monitor, and extract insights from cross-platform testing in near real time through a centralized observability platform.
Cross-platform testing validates that an application works correctly across the full range of devices, operating systems, browsers, and environments users access it from. The goal is to confirm consistent functionality, performance, and visual quality regardless of how users reach the application. Modern cross-platform testing uses AI computer vision to interact with applications the same way users do, eliminating the need for separate test scripts per platform and extending coverage to environments where source code access is restricted.
Cross-browser testing is a subset of cross-platform testing focused specifically on validating that web applications work correctly across browsers like Chrome, Safari, Firefox, and Edge. Cross-platform testing is broader, covering operating systems, device types, mobile and desktop applications, mainframes, and packaged software in addition to browsers. For most modern enterprises whose user experience extends beyond web browsers, cross-platform testing is the more relevant scope. Cross-browser testing alone misses the platform breadth most applications now span.
With AI-driven computer vision, yes. Traditional automation tools require separate scripts per operating system because they depend on platform-specific selectors, accessibility APIs, or DOM structure. AI-driven visual testing platforms interact with applications by what's on screen rather than how it's coded, which means a single test definition can run across Windows, macOS, Linux, iOS, Android, and even mainframe environments. This dramatically reduces the per-platform effort historically required to maintain comprehensive cross-platform coverage.
AI-powered visual testing enables cross-platform automation by removing the technology-stack dependencies that traditionally fragmented testing approaches. Instead of relying on platform-specific selectors or back-end APIs, AI computer vision recognizes UI elements by appearance, the same way users do. This means the same test logic works whether it's running against a web browser, a mobile app, a desktop application, a mainframe terminal, or a packaged software interface. The result is consistent automation coverage across an enterprise application portfolio without per-platform tooling.
The best approach to combined mobile and desktop coverage depends on the consistency required across platforms. If mobile and desktop are tested by separate teams with different processes, specialized tools per platform may work. For organizations where the same workflows need consistent validation across mobile and desktop, AI-driven visual testing platforms deliver lower total maintenance overhead by using one test approach across both. The right choice depends on whether unified coverage or specialized per-platform depth is the higher priority.
Testing applications without source code access requires moving away from automation approaches that depend on DOM, accessibility APIs, or instrumentation hooks. AI-driven visual testing works by interacting with applications through the visible UI, the same channel users use, which means it doesn't require source code access at all. This makes it particularly valuable for packaged software, mainframe applications, third-party systems, and locked-down environments where traditional automation tools can't reach. The same test approach extends to applications you do control, providing consistent coverage across the full estate.
무엇을 찾고 있습니까?