Standards-Related Trademarks for which Acknowledgements are Mandated

This is a list of standards-related trademarks that Keysight is contractually obligated to acknowledge as a condition of membership in the relevant standard setting organization.

Trademark  Acknowledgement 
AdvancedMC™
AdvancedMC logo+™
AdvancedMC™ and the AdvancedMC logo are trademarks of the PCI Industrial Computer Manufacturers Group.
AdvancedTCA®
ATCA®
ATCA logo +®
ATCA®, AdvancedTCA®, and the ATCA logo are registered US trademarks of the PCI Industrial Computer Manufacturers Group.
Bluetooth®
Bluetooth logo®
Bluetooth® and the Bluetooth® logos are registered trademarks owned by Bluetooth SIG, Inc., and any use of such marks by Keysight Technologies is under license
cdma2000® cdma2000® is a US registered certification mark of the Telecommunications Industry Association.
COM Express™
COM Express logo+™
COM Express™ and the COM Express logo are trademarks of the PCI Industrial Computer Manufacturers Group.
CompactPCI®
CompactPCI logo+®
CompactPCI® and the CompactPCI logo are registered US trademarks of the PCI Industrial Computer Manufacturers Group.
CompactTCA™
CompactTCA logo+™
CompactTCA™ and the CompactTCA logo are trademarks of the PCI Industrial Computer Manufacturers Group.
EMV™ EMV™ is a trademark owned by EMVCo LLC. www.emvco.com
Infineon Infineon is a registered trademark of Infineon Technologies AG.  The Infiniium mark is used with the kind approval of Infineon Technologies, AG.
LTE logo
LTE-Advanced logo
LTE logo and LTE-Advanced logo are trademarks of ETSI.
MicroTCA™
MicroTCA logo+™
MicroTCA™ and the MicroTCA logo are trademarks of the PCI Industrial Computer Manufacturers Group.
M-PHY®
MIPI®
SLIMbus®
DigRF®
UniProSM
D-PHYSM
C-PHYSM
MIPI® service marks and logo marks are owned by MIPI Alliance, Inc. and any use of such marks by Keysight Technologies is under license. Other service marks and trade names are those of their respective owners.
NVM Express™
NVMe™
Associated Logos
The NVM Express™ design mark and NVMe™ word mark are trademarks of NVM Express, Inc.
PCI-SIG®
PCI EXPRESS®
PCIe®
PCI-SIG®, PCIe® and the PCI Express® are US registered trademarks and/or service marks of PCI-SIG.
PICMG ®
PICMG logo+®
PICMG® and the PICMG logo are registered US trademarks of the PCI Industrial Computer Manufacturers Group.
SHB Express™
SHB Express logo+™
SHB Express™ and the SHB Express logo are trademarks of the PCI Industrial Computer Manufacturers Group.
SS USB Trident Logo
USB PD Logo
The SuperSpeed USB Trident logo is a registered trademark of USB Implementers Forum, Inc.
The USB Power Delivery logos are trademarks of USB Implementers Forum, Inc.
Wi-Fi® Wi-Fi® is a registered trademark of the Wi-Fi Alliance®
WiMAX™
WiMAX Forum®
WiMAX Forum logo
Mobile WiMAX™
WiMAX Forum
Certified™
WiMAX Forum Certified logo
Fixed WiMAX™
Fixed WiMAX™, WiMAX™, Mobile WiMAX™, WiMAX Forum®, the WiMAX Forum logo, WiMAX Forum Certified™,  and the WiMAX Forum Certified logo are US trademarks of the WiMAX Forum.
X-parameters* *X-parameters is a trademark and registered trademark of Keysight Technologies in the US, EU, JP, and elsewhere.
ZigBee®
ZigBee logo

Place the ZigBee logo prominently and keep it separate from the other type and symbols.

In headlines or text, typeset the ZigBee® name with the Registered ® trademark symbol for first reference. Do not use the logo artwork.

Use as adjective with a noun - for example, use “ZigBee Alliance,” “ZigBee Specification” or “ZigBee Standard.”

The word ZigBee may not be used as a modifier in conjunction with adjectives. Terms such “ZigBee compatible” or “ZigBee ready” or “ZigBee enabled” create confusion with regard to certification and standards. It is unacceptable to use the word ZigBee, or any derivation of the word ZigBee to name products or services.

Keysight reserves the right to discontinue use of a given acknowledgement after due consideration of any business relationship with the trademark owner, the accuracy of the acknowledgement, the quality and strength of the trademark, third-party claims, and other factors.