솔루션 개요
It is estimated that 85% of mean time to repair (MTTR) is consumed by simply trying to verify that there is, in fact, an issue. What if you could change this? Context-aware data processing can be used to help IT in this area. By reducing the discovery time for network issues, the MTTR is automatically reduced.
This solution brief provides a general overview of how application intelligence can improve network and application troubleshooting and monitoring functions. In addition, a clear example is provided to illustrate how IT can change the focus of troubleshooting from reactive efforts to proactive efforts to help reduce time and cost.
무엇을 찾고 있습니까?