何をお探しですか?
EDA Integrations
Built into the tools engineers love - Keysight SOS lives inside your EDA environment - no switching, no friction.
Why Native Integration Changes Everything
Let me tell you something that nobody in the EDA world wants to admit: we're killing engineering productivity one context switch at a time. Every time an engineer has to leave their design environment to check in a file, update a status, or trace a dependency, we're not just wasting seconds — we're shattering flow state. And flow state is where genius happens.
Engineers aren't forgetful. They're human. When you force them to juggle five different tools to complete one workflow, errors don't just happen — they're inevitable. A missed check-in here, a version mismatch there, and suddenly your tapeout schedule is in jeopardy. Worse yet, every manual data transfer between tools is a security incident waiting to happen. Data leakage isn't dramatic — it's death by a thousand clipboard copies, imports, and exports.
This isn't about convenience. It's about respect for the craft. When tools talk to each other natively, engineers can focus on what they were hired to do: design breakthrough products that change the world. Everything else? That's just friction we've been too lazy to eliminate.
Your Entire Toolchain, Already Connected
SOS doesn't just claim to integrate with EDA tools — we actually do the work. Every major platform your team depends on, connected natively. No adapters, no middleware hell, no excuses.
What Native Menu Integration Really Means
Here's the beautiful part: your engineers won't need training. They won't need to read documentation. They won't need to remember new commands. SOS appears right where they expect it — in the menus they already use every single day.
Check-In / Check-out Inside the Tool
Version control lives in the File menu. Right-click to check out a design. Save to check in. It's that simple. No separate application, no command line, no interruption to your workflow.
Automatic Metadata Capture
Who designed it? What process node? Which revision? What simulation corner? SOS captures all of it automatically. Engineers design, SOS documents. That's the deal.
Automatic Traceability
Every schematic links to its layout. Every layout links to its LVS run. Every simulation connects to its testbench. The audit trail builds itself while engineers work, creating a web of dependencies that answers "what changed and why" in seconds, not days.
Governance Without the Overhead
Compliance isn't something engineers do — it's something that happens automatically. Access controls, change tracking, approval workflows — all enforced transparently. Engineers focus on design. Managers sleep soundly. Auditors find everything they need.
SOS Lives Inside Your Toolchain
SOS Core: Central system with secure repository and audit.
It allows:
- Native integration with Cadence tools
- Native connectivity with Synopsys tools
- Native integration and seamless exchange of Keysight data
- Bidirectional sync with Siemens EDA tools
Purpose-Built for Real Workflows
SOS doesn't just integrate with tools — it understands the actual work engineers do. These aren't theoretical use cases. They're real workflows at real companies designing real products that ship in real volume.
Analog Design
From initial topology exploration through final characterization, every design iteration tracked. Schematic versions linked to simulation results. Corners documented. Performance trends visible. When a design meets spec, you know exactly which configuration got you there.
Physical Layout
Layout cells under version control from first placement. DRC/LVS runs tracked against specific layout revisions. When physical verification fails, you don't hunt for which version had the problem — SOS tells you instantly.
EM Simulations
Electromagnetic analysis results linked to the exact layout and stackup that generated them. Parameter sweeps documented. Correlation between EM extraction and circuit simulation maintained automatically. No more "which extraction file did we use for this tape-out?"
RF Workflows
From system architecture in MATLAB through transistor-level design in ADS to layout verification — the entire RF flow connected. S-parameters linked to layouts. Matching networks versioned with their performance data. Tapeout packages assembled correctly, every single time.
What Engineers Actually Get
Let's cut through the enterprise software nonsense and talk about what matters to the people doing the actual work. Engineers don't want features — they want their day back. They want to spend time designing, not administering tools. SOS delivers exactly that.
No context switching
Design in Virtuoso. Stay in Virtuoso. Check-in happens in Virtuoso. Version history appears in Virtuoso. Everything lives where you're already working. Your flow remains unbroken.
No cognitive overhead
You don't think about version control. You don't remember to capture metadata. You don't manually link dependencies. The system handles all of it transparently while you focus on the design problem you're actually trying to solve.
Just designing and testing
You were hired because you're brilliant at circuit design or physical layout or EM analysis. SOS ensures you spend your time doing exactly that — not fighting tools, not hunting for files, not reconstructing history. Just engineering.
What Engineering Managers Actually Need
You're measured on schedules, quality, and compliance. Your team is measured on design excellence. SOS ensures both sets of goals align perfectly instead of conflicting. Here's what you get without asking your engineers to do extra work:
Complete Audit Trails
Every design change documented automatically. Who modified what, when, and why — captured without engineers filling out forms or writing commit messages. When the auditor asks "show me the history of this critical net," you pull up the complete record in 30 seconds.
End-to-End Traceability
Requirements trace to schematics. Schematics trace to layouts. Layouts trace to verification runs. Verification traces to tapeout. The entire design lineage visible in one system. When a customer issue emerges post-silicon, you identify the root cause in minutes instead of weeks.
Security that Actually Works
Access controls enforced at the tool level. No way to bypass them. No manual copying of files to unsecured locations. IP stays protected because the system architecture makes data leakage physically difficult. Security through design, not through policy documents nobody reads.
Compliance Readiness Built-In
ISO 26262, ITAR, export control, customer audit requirements — all the regulatory burdens that keep you up at night become straightforward when your toolchain maintains evidence automatically. SOS doesn't make compliance easy — it makes compliance invisible.
The brilliant part? Your engineers never feel micromanaged. They're not filling out status reports or tracking their work manually. They're just designing — and the system you deployed makes governance automatic. That's leadership.
Ready to Eliminate Tool Friction Forever?
You have two choices. You can keep accepting context switching, manual tracking, and preventable errors as "just how semiconductor design works." Or you can deploy SOS and give your team the integrated toolchain they deserve.
SOS Core provides native EDA integrations with version control, traceability, and governance for teams building breakthrough products. SOS Enterprise adds enterprise-grade security, compliance automation, and global deployment capabilities for organizations with complex regulatory requirements.
Both eliminate the friction that's slowing your team down. Both respect engineering talent by removing administrative burden. Both ship with the native integrations that make adoption instant.
The question isn't whether native EDA integration matters. The question is how much longer you're willing to let tool friction slow down your most valuable resource: your engineering team.
Learn More
Featured Resources
Want help or have questions?