Sharing IP-Protected Nonlinear Behavioral Models Using X-Parameters

アプリケーションノート

RF system design is a notoriously complex and challenging endeavor, made even more so by today’s stringent time-to-market requirements. Meeting these requirements places increasing pressure on system integrators to speed the system-design process wherever possible. One viable option for addressing these concerns lies in the ability to evaluate real circuit-level designs from design houses/component vendors within the system context, early in the design process and prior to the availability of a physical hardware prototype.