EP-Scan for PI Applications

デモ

Ensure reliable power delivery network (PDN) design by analyzing DC IR-drop during the layout phase, improving power integrity visibility.

 

By the end of this session, PCB designers can:

 

  • Create and configure power delivery networks
  • Define sources and sinks with voltage and current conditions
  • Evaluate voltage limits using pass/fail criteria
  • Analyze DC IR-drops across the power network
  • Visualize current density and voltage distribution
  • Identify high current paths and potential hotspots