Shifting Reliability Left: Guided Virtual Validation for Electronics Shock and Drop Testing

白書

Mechanical shock failures remain one of the most disruptive and expensive challenges in electronics product development. When identified during physical qualification testing, design changes are often costly, time-consuming, and constrained by frozen hardware. While traditional CAE simulation can help identify structural weaknesses earlier, it typically requires specialized expertise that is unavailable to many engineering teams, limiting its adoption during the design phase.

 

This white paper explores how guided virtual shock analysis bridges the gap between early design flexibility and reliable structural qualification. Using Keysight Multiphysics, design engineers can perform system-level drop and impact simulations through a template-based workflow that eliminates much of the complexity associated with conventional CAE tools. Standardized validation plans automate execution of the complete drop orientation matrix in a single run, while built-in reporting delivers decision-ready results directly from the simulation environment.

 

The approach enables engineering teams to identify shock-sensitive load paths, packaging weaknesses, and structural risks before hardware is committed, when design modifications are faster and more cost-effective. Engineers can evaluate packaging durability and structural response across multiple impact orientations, compare design alternatives, and optimize product robustness through virtual iteration rather than repeated physical prototypes.

 

The white paper also demonstrates the predictive accuracy of the solution through correlation with physical drop testing on representative packaged electronics. By accurately modeling the complex material combinations and assembly interactions found in modern electronic products, guided virtual shock analysis provides confidence in simulation results while accelerating development, reducing prototyping costs, and improving product reliability.