O que você está procurando?
S97088B Source Phase Control
Set calibrated, arbitrary phase differences between two signal sources running on the P50xxA Streamline VNAs.
A partir de
The S97088B allows users to set calibrated, arbitrary phase differences between two signal sources running on the P50xxA Streamline VNAs.
Highlights
- Control the relative phase between the two internal sources and/or external signal generators
- Provide calibrated, electronic loads to an amplifier under test
- Sweep the phase of the load while maintaining the constant reflection-coefficient magnitude
- Requires 2 or more sources configurations, such as 2 modules stacked configurations or the internal 2 source configurations (P50xxA-4X2)
The S97088B allows users to set calibrated, arbitrary phase differences between two signal sources. The sources can be the analyzer’s internal sources or external signal generators routed through the analyzer’s test set. The phase difference can be fixed, or swept between two specified phase values. S97088B also controls the relative power level between the sources using the receiver-leveling feature.
The S97088B is targeted for active-load control, where the analyzer provides a precise, electronically settable impedance to the output port of a device, while gain and output power are measured. This capability can be combined with external load-pull software to create traditional load-pull power contours.
Amplie as Capacidades
Want help or have questions?