O que você está procurando?
KS9802HMNB PathWave Measurements Noise Figure Analysis Pack
Measure one of the key components of receiver sensitivity with noise figure
A partir de
Identify the key contributors to your receivers sensitivity, by measuring the noise figure of your device or network.
Highlights
The KS9802HMNB PathWave Measurements Noise Figure Analysis Pack includes:
- Hardware control of noise source
- Hardware control of PXIe signal analyzer
- Support for 2 noise figure estimation methods: Y-factor and Cold Source
- Calibration method and previous calibration recall
- Noise figure and gain results
The KS9802HMNB PathWave Measurements Noise Figure Analysis Pack enables the measurement of device or network noise figure by controlling test equipment to supply a noise signal to the device and measuring the device response from a PXIe receiver. By definition, the noise figure of a network is defined as the ratio of the signal-to-noise ratio (SNR) at the input to the SNR at the output. The most typical device-under-test (DUT) is an amplifier.
Amplie as Capacidades
Want help or have questions?