Article Reprints
Keysight Technologies
The Boundary Scan Toolbox
Article Reprint
The Boundary Scan Toolbox
Enabling embedded and other value-added test in your toolbox.
The popularity of boundary scan (IEEE 1149.1) has been increasing through the years to become one of the preferred methods of electronics manu-facturing testing of printed circuit board assem-blies. Boundary scan is commonly used as a lim-ited access solution for high-node-count PCBAs (10,000 to 20,000 nodes). Due to component density on board, it is typically either not possible or too costly to test such PCBAs using in-circuit test (ICT) bed-of-nails solutions. Over the years, the typical boundary scan toolbox has expanded to include shorts test-ing, voltage measurement testing, Cover-Extend, embedded BIST (built-in self-test) and Intel Silicon View Technology.
Structural shorts test. The integrated boundary scan toolbox is not a substitute for an ICT shorts and opens test, which can detect shorts for all accessible nodes. However, boundary scan offers the ability to selectively check for a possible short by measuring the resistance between power nodes, where a short will cause a catastrophic failure (FIGURE 1) to a PCB when the circuit board is powered on. This is a very welcome addition for manufacturing test folks who need to avoid costly damage to the PCBA.
Voltage measurement. Ensuring the correct power-up voltage for the PCBA is another impor-tant part of the boundary scan toolbox. This measurement ensures the boundary scan test will not fail due to inadequate voltage levels of the boundary scan devices, something that can be hard to diagnose, as the test engineer will not get a straightforward failure message to indicate that a power rail is faulty.
Cover-Extend Technology. CET is a hybrid between VTEP (vectorless test enhanced performance) and bound-ary scan. It enhances the overall capability of the boundary scan tool by enabling structural tests on non-boundary scan devices such as connectors that are connected to a boundary scan device. The technology works as follows:
Embedded test (BIST and Intel SVT). Built-in self-test (BIST) has been gaining ground in the industry with the recent passing of the IEEE 1149.1 2013 and IEEE 1687 standards, both of which support embedded testing. BIST has been around for some time, but had been mostly implemented only at the chip level. Implementation of on-board test was not widespread, mainly due to lim-ited availability of BIST support at the board level from boundary scan device vendors. Since then, boundary scan tools have included STAPL/SVF to enable support on vari-ous devices with instruction “opcodes” for BIST testing.
Intel SVT requires the BIOS to be set up according to Intel BIOS Writer Guide3, reserving a designated reg-ister to host the results of the Intel SVT test. During manufacturing test, the PCBA under test has to be pow-ered up safely to run the BIOS, and Intel SVT will post the results of its test into the designated register. The content of the register is then com-pared to known good board values to assess whether the PCBA passes or fails the set of tests.
Intel SVT will test the following via the Haswell CPU (and BIOS):
Continued advancement of both software and hardware in the bound-ary scan toolbox and concurrent development and support of industry standards will help to regain test cov-erage lost on traditional ICT meth-ods. In the near future, the handy boundary scan toolbox is likely to expand with new features to exceed the expected test coverage of today’s complex PCB assemblies.
O que você está procurando?