Demonstrações
This demonstration video, presented by Kenny, a product manager at Keysight Technologies, provides a comprehensive walkthrough on how to simulate Lithium Iron Phosphate (LiFePO₄) battery cells using the Keysight Smart Bench Essentials Plus (SBE+) 4-channel DC power supply to test and validate the auto-balancing functionality of a Battery Management System (BMS). The video, approximately 3 minutes and 30 seconds in duration, is designed to help engineers and developers ensure the reliability and safety of BMS units used in electric vehicles and energy storage systems.
The demonstration begins by explaining the importance of BMS in managing cell imbalances that naturally occur over time due to manufacturing variances, temperature fluctuations, and aging. These imbalances can lead to reduced battery life, decreased performance, and potential safety hazards. A robust BMS must detect and correct these imbalances through active or passive balancing mechanisms. Validating this functionality is critical before integrating the BMS into a full battery pack.
To simulate real-world conditions, the setup uses the Keysight E36441A 4-channel DC power supply to represent four individual battery cells. Each channel is configured to output 3.6 volts with a current limit of 2 amps—typical values for LiFePO₄ cells. The power supply’s precision and flexibility make it ideal for this application, allowing each channel to be independently controlled and monitored.
The demonstration proceeds with a detailed setup of the power supply and its connection to the BMS. Each output channel of the power supply is connected to a corresponding input on the BMS, effectively simulating a 4-cell battery pack. The video highlights the use of the power supply’s output sequencing feature to stagger the activation of each channel, preventing inrush currents that could damage the BMS.
A key feature showcased is the LIST mode, which allows the simulation of voltage imbalances by programming a sequence of voltage levels over time. This triggers the BMS’s auto-balancing function, which is then monitored using the Smart BMS mobile app and the power supply’s data logger. The data logger captures real-time voltage fluctuations, providing visual confirmation of the BMS actively correcting the imbalance.
The final segment reviews the results and emphasizes the benefits of using the SBE+ power supply for BMS testing. The ability to simulate multiple cells with a single instrument simplifies the test setup and reduces equipment needs. The power supply’s high configurability and real-time monitoring capabilities make it a powerful tool for validating BMS performance under controlled, repeatable conditions.
In conclusion, the video demonstrates how Keysight’s Smart Bench Essentials Plus 4-channel DC power supply enables efficient and accurate simulation of battery cells for BMS testing. This approach not only ensures the safety and reliability of battery systems in electric vehicles but also accelerates development cycles by providing engineers with a flexible and precise testing platform.
O que você está procurando?