Hardware-Driven Mixer Behavioral Modeling with the VanDyke Mixer in SystemVue

Notas de Aplicação

Frequency translation is fundamental to virtually every RF transmitter and receiver, yet accurately predicting mixer spurious outputs remains one of the most challenging aspects of system-level simulation. For nearly four decades, engineers have relied on the Intermod Mixer Table (IMT) to represent mixer behavior. While the IMT helped advance RF electronic design automation, today's increasingly complex systems require behavioral models that are easier to characterize, more intuitive to use, and capable of reproducing real hardware performance with greater fidelity.

 

This application note introduces the VanDyke mixer, a hardware-driven behavioral mixer model available in the Spectrasys simulator within Keysight SystemVue 2026. The model replaces traditional index-based intermodulation tables with a measurement-native equation format, enabling engineers to create an RF digital twin directly from measured mixer behavior.

 

Using a Pulsar X2L-10-411 double-balanced mixer, the application note demonstrates the complete measurement-to-simulation workflow. The physical mixer is first characterized using a Keysight PNA-X network analyzer. Its measured output spectrum peak table is saved in the Keysight Mixer Spur Data MDF format before the Mixer Data Tool converts the measurement data into mixer equations for use in Spectrasys. The resulting behavioral model reproduces the measured output spectrum peak for peak, including actual spurious signals and leakage observed in the physical device.

 

This streamlined workflow allows engineers to move from bench measurements to a reusable behavioral model in minutes. Rather than manually constructing and interpreting complex intermodulation tables, designers can build simulation models grounded directly in measured hardware performance.