Solution Briefs
In today’s continuously evolving digital landscape, enterprise applications and systems are under relentless pressure to stay current. Operating systems, APIs, and third-party integrations update at an unprecedented pace – promising progress but also introducing risk. Each patch or upgrade can alter workflows, disrupt integrations, or compromise user experience. Testing every change is essential, yet traditional regression methods — whether manual or script-based — struggle to keep up, creating bottlenecks that slow innovation and heighten operational risk.
Keysight Eggplant Test transforms the challenge of updates and upgrades into an opportunity for continuous quality assurance. Combining AI-assisted modeling, visual automation, and cross-version validation, Eggplant enables teams to test faster, smarter, and more reliably across desktop, web, mobile, and virtual environments. Unlike brittle, code-dependent scripts, Eggplant interacts with systems visually, just as a human user would, making it resilient to UI changes and version differences. Its intelligent comparison engine can run side-by-side validations between versions, identify functional or visual discrepancies, and ensure that every workflow — from data handling to end-user experience — remains consistent after each release.
Through AI-driven insights and model-based automation, Eggplant helps QA teams target only the areas affected by change, drastically reducing redundant testing. Continuous integration support embeds automated validation into every deployment pipeline, turning regression testing into a proactive, ongoing safeguard. With business-level reporting, stakeholders can understand not only what changed but also which workflows or customer journeys are impacted — closing the gap between QA, DevOps, and leadership.
The results are measurable. Enterprises adopting Eggplant have seen up to a 70% reduction in regression effort, 50–60% faster validation cycles, and significantly fewer post-release defects. Siemens Digital Industries, for example, cut regression testing time by 66%, reduced manual dependencies, and uncovered critical defects before release — improving both release confidence and product quality. Other organizations, such as Keysight IT and MCB Temenos, accelerated upgrade projects by up to 3×, reduced stabilization time by 80%, and achieved continuous assurance across complex, multi-platform systems.
For QA engineers, Eggplant minimizes repetitive maintenance and enables focus on exploratory and strategic testing. For testing managers, it provides transparency, traceability, and efficiency through targeted coverage and visual reporting. For executives, it ensures faster, safer adoption of innovation — turning upgrades from a source of risk into a driver of competitive advantage.
Ultimately, Eggplant enables enterprises to evolve without fear. Every patch, platform migration, and version release becomes an opportunity to strengthen quality, enhance resilience, and accelerate delivery. By embedding AI-powered automation into the update lifecycle, organizations achieve what Eggplant calls continuous confidence — a state where innovation and reliability advance in sync.
O que você está procurando?