Solution Briefs
As banks and financial institutions around the world seek to modernize legacy infrastructure and meet growing customer demands, rigorous testing of core banking systems is critical to ensuring seamless digital transformation. Temenos T24, one of the world’s leading core banking systems, serves over 950 institutions globally. However, testing Temenos deployments presents unique challenges due to the complexity of integrations, frequent system updates, and the need for real-time performance across channels such as ATMs, POS systems, and Internet Banking. Eggplant Test, a Keysight solution, offers a robust and intelligent testing platform tailored to the demands of Temenos environments.
Eggplant Test brings a modern, AI-driven approach to Temenos testing. Using advanced object recognition and intelligent automation, Eggplant executes end-to-end tests from the user’s perspective. This method ensures that test coverage is both comprehensive and realistic, reflecting how customers and employees interact with the system. Because Eggplant is resilient to changes in the user interface, tests are more stable and require less maintenance—even as Temenos updates or interface elements evolve.
The solution supports virtual and remote testing environments, enabling QA teams to execute tests securely from anywhere. By supporting both physical systems and virtual environments like VMs and VNC, Eggplant ensures consistent quality and reliability regardless of infrastructure. Side-by-side comparisons between real and virtual environments further bolster confidence in deployment outcomes.
To maximize testing success, Eggplant promotes strategic best practices. These include aligning testing initiatives with broader business goals, phasing implementations to prioritize critical functions, instituting strong governance frameworks, and executing comprehensive performance, security, and user acceptance testing throughout the project lifecycle.
Eggplant is uniquely positioned to address key Temenos testing challenges. Its UI-agnostic and model-based testing approach ensures coverage of complex integrations across banking modules. Frequent updates to the Temenos platform, which can often disrupt traditional test scripts, are handled gracefully through Eggplant’s AI-powered automation, which focuses on user journeys rather than rigid scripts. Additionally, Eggplant supports data-driven testing through integration with databases, APIs, and spreadsheets, ensuring that the test inputs and validations reflect real-world scenarios and maintain data integrity.
Proven customer success underscores the value of Eggplant Test for Temenos environments. For example, the Mauritius Commercial Bank leveraged Eggplant to reduce regression testing time from 400 days to 120 and achieved 70% test automation coverage. These results highlight Eggplant’s ability to streamline testing operations, reduce manual effort, and accelerate time-to-value.
In conclusion, Eggplant Test provides a powerful and intelligent testing solution tailored to the demands of modern Temenos deployments. With capabilities such as AI-powered test automation, robust object recognition, support for virtual environments, and data-driven testing, Eggplant enables banks to confidently deliver high-quality, compliant, and user-centric digital banking experiences. By adopting Eggplant, financial institutions can overcome testing challenges and ensure the reliability, security, and performance of their core banking operations.
O que você está procurando?