Folhetos
NB-IoT NTN Device Acceptance
Protocol, RF and functional test solutions
Ensure chipset and devices comply to 3GPP and Satellite Network Operator certification test
Non-Terrestrial Networks (NTN) offer wireless connectivity through satellite and satellite constellations and can be used standalone or as a complement to traditional Terrestrial Networks (TN). The latter is an interesting use case for commercial communications based on 5G as it permits extending the coverage to the complete globe without access restrictions in remote areas and oceans which have been out of reach so far. Besides global coverage another advantage is a greater resilience to natural disasters and network damages in conflict areas, which ensure access to wireless communication to emergency services.
The use of satellite networks is facilitated by the evolution of the satellite technology with lower cost of operation now. There are different types of satellite networks depending on the orbit altitude and latitude.
• Geostationary or GEO, with satellites located approx. 36000 km altitude and appearing nearly stationary to a ground observer and have same orbital period as the earth. The orbit is in the plane of the equator, with 0º degrees inclination. GEO with its high orbital altitude has a long delay in the communication to ground, although such delay is fix and therefore easier to compensate. These satellites are relatively expensive and have few available orbits.
• Geosynchronous or GSO, is a special case of GEO with a variable inclination e.g., orbital tilt relative to the equator. GSO have more orbit opportunities and therefore can be used by a greater number of satellite operators. Delay and also frequency shift due to doppler effect vary during the orbit and devices must be designed to do the proper compensation to ensure coverage.
• Non-Geosynchronous or NGSO, consist of low flying satellites with orbit time less than 24h, often referred as LEO for Low Earth Orbit. The advantage is fast and lower cost deployment at the expense of offering only discontinuous coverage and requiring more precise compensation of the delay and doppler by the devices.
As with other features, to ensure NTN meets the service providers and user expectations, global specifications and test specifications are needed as well as certification programs which can prove compliance of devices. With the evolution of 5G NR different device form factors can be subject to testing from mobile phones to wearables, and IoT sensors and actuators.
3GPP Release 17 already supports NTN. The work is about to finalize for 3GPP test specifications for Protocol and RF/RRM test cases with priority first in NB-IoT NTN followed by NR NTN. Additionally, some Satellite Network Operators have their own certification programs. It is the case of Skylo who is supporting 3GPP Release 17 standards and working on specific supplementary test to ensure good performance of the devices on their network.
Keysight Device Acceptance Solutions support NTN Conformance and Carrier acceptance requirements.
• 3GPP Protocol Test Cases based on 36.523-1
• 3GPP Transmitter and Receive Test Cases based on 36.521-4
• 3GPP Demodulation Performance Test Cases based on 36.521-4
• 3GPP Radio Resource Management (RRM) Test Cases based on 36.521-3
• Skylo’s NB NTN Certification test cases (Sep’23 release)
O que você está procurando?