キーサイト公式
再生品ストア

Oscilloscope Glossary

What Is a Spectrum Analyzer? A Beginner's Guide

Table of contents
Callum Reed
Used Equipment Store Marketing Manager
ご意見・ご感想をお寄せください
Stay Up to Date on Used Equipment!

Don’t miss special offers, news, and announcements on the latest used equipment. Unsubscribe at any time.

Get Email Updates
Second-Hand. First-Class.

Don’t miss special offers, news, and announcements on the latest used equipment. Unsubscribe at any time.

Why Buy From Keysight

Signal Analyzers

Rugged Precision, Anytime

See N9020 Special Offers

Introduction

A spectrum analyzer shows how a signal's amplitude varies across different frequencies. While an oscilloscope shows how a signal changes over time, a spectrum analyzer helps you identify frequency components, harmonics, and interference.

This guide explains how spectrum analyzers work, the main types available, and how to take your first measurement. For help comparing models, see the spectrum analyzer buying guide.

Overview
  • A spectrum analyzer displays signal amplitude against frequency. An oscilloscope displays amplitude against time.
  • Swept-tuned analyzers scan a frequency range using a narrow filter. FFT-based analyzers calculate the spectrum from digitized signals, while real-time analyzers continuously process signals within their specified analysis bandwidth.
  • Four settings shape most initial measurements: span, resolution bandwidth (RBW), reference level, and input attenuation. State the RBW with every noise reading.
  • A spectrum analyzer measures a signal's frequency content. To measure how a component responds to an applied signal, including its phase response, use a vector network analyzer (VNA) such as the used Keysight E5071C, which offers frequency coverage up to 20 GHz.

What Is a Spectrum Analyzer?

A spectrum analyzer shows the frequencies present in an electronic signal and measures their levels. While an oscilloscope displays how a signal changes over time, a spectrum analyzer helps you identify frequency components such as harmonics and unwanted signals. Engineers use it for radio frequency (RF) testing and diagnosing electromagnetic interference (EMI).

Many modern signal analyzers combine traditional spectrum measurements with more advanced capabilities, such as analyzing complex or modulated signals, depending on their installed software and options. This guide uses "spectrum analyzer" to refer to both.

A spectrum analyzer typically measures signals without supplying its own test stimulus. Some models include an optional tracking generator for basic magnitude-only response measurements. To measure a component's response, including both magnitude and phase, a vector network (VNA) is generally the better choice. The used Keysight E5071C offers frequency coverage up to 20 GHz, while Keysight recommends the E5080B for new purchases.

Keysight 8565EC spectrum analyzer
A Keysight 8565EC spectrum analyzer, a discontinued model that Keysight lists as obsolete. Source: Keysight.

How Does a Spectrum Analyzer Work?

A swept-tuned spectrum analyzer scans a range of frequencies and measures the signal level at each one, creating a display of amplitude versus frequency. Keysight's guide How Does a Spectrum Analyzer Work? explains the mixer and detector stages. The main stages are:

  • Input attenuator: Reduces the signal level before it reaches the input mixer.
  • Mixer and local oscillator (LO): The local oscillator produces a signal that mixes with the incoming signal, converting selected frequency components to an intermediate frequency (IF). As the LO sweeps, different frequency components pass through the IF stage.
  • IF filter: Passes a narrow band of frequencies. The filter's width determines the resolution bandwidth (RBW).
  • Detector and video filter: The detector measures the level of the filtered signal, while the video filter can smooth the displayed trace.
  • Display: Shows the measured signal level against frequency.
Block diagram of a swept-tuned spectrum analyzer: RF input passes through an input attenuator, a mixer, an IF filter marked RBW, a detector and video filter, and a display showing a single peak; a local oscillator below the mixer feeds it, with its arrow marked sweeps
The local oscillator sweeps, so each part of the span passes through the IF filter in turn; the filter's width is the resolution bandwidth (RBW). Source: Keysight illustration. | spec: block diagram, not a data chart. Five blocks left to right: input attenuator, mixer (with a local oscillator block feeding it from below, labeled "sweeps"), IF filter (labeled "RBW"), detector with video filter, display (showing a single peak, labeled "amplitude versus frequency"). Units: none. Data source: Sources 1 (mixer, LO, filter, detector), 3 (RBW is the IF filter bandwidth; VBW smooths the trace) and 11 (input mixer level, so the attenuator sits before the mixer).

What Are the Types of Spectrum Analyzers?

The right type depends on the signals you need to see. Frequency range varies by model, so check the data sheet for the analyzer you're considering.

1. Swept-Tuned Spectrum Analyzers

Swept-tuned analyzers are the traditional design. The local oscillator (LO) sweeps so the analyzer tunes across the selected frequency span, while the intermediate frequency (IF) filter determines the resolution bandwidth. Newer swept analyzers use digital signal processing, so check the data sheet for how a given model works.

  • Simple signal path: The block diagram above shows the main stages from input to display.
  • One narrow band at a time: At any instant the analyzer measures only the narrow band it is tuned to, so a short event elsewhere in the span can be missed.
  • Resolution depends on the filter: Closely spaced signals need a narrow RBW, which slows the sweep.

2. Digital Spectrum Analyzers

Digital spectrum analyzers convert incoming signals into digital data for processing. A common method is the Fast Fourier Transform (FFT), which calculates the spectrum of a captured time-domain signal.

  • Whole band at once: An FFT analyzer can compute many frequencies from one capture instead of stepping through them one at a time.
  • Vector signal analyzers: With vector analysis software, a signal analyzer can examine complex signals, such as modulated carriers.

3. Real-Time Spectrum Analyzers

A swept-tuned analyzer measures one narrow band at a time, so it can miss what happens elsewhere in the span. A real-time spectrum analyzer processes every sample within a stated bandwidth without gaps. Keysight's 89600B help describes a swept-tuned analyzer as displaying results sequentially and a real-time analyzer as displaying the energy at all frequency components simultaneously.

  • Short events: Useful for intermittent interference and signal bursts that can be shorter than a sweep.
  • Limits: The analysis bandwidth and the shortest event the analyzer can show depend on the model, so read the specification for the one you plan to use.

How the Three Types Compare

Type How it measures Strength Limit
Swept-tuned Sweeps the span past a narrow IF filter Simple signal path Sees one narrow band at a time
Digital (FFT-based) Digitizes the signal and calculates the spectrum Can compute a whole band from one capture Captures are bounded by the analysis bandwidth
Real-time Processes every sample in a stated bandwidth without gaps Short events inside the bandwidth Analysis bandwidth depends on the model
Type
How it measures
Strength
Limit
Swept-tuned
Title
Sweeps the span past a narrow IF filter
Title
Simple signal path
Title
Sees one narrow band at a time
Digital (FFT-based)
Title
Digitizes the signal and calculates the spectrum
Title
Can compute a whole band from one capture
Title
Captures are bounded by the analysis bandwidth
Real-time
Title
Processes every sample in a stated bandwidth without gaps
Title
Short events inside the bandwidth
Title
Analysis bandwidth depends on the model

What Can a Spectrum Analyzer Measure?

A spectrum analyzer measures the frequency and amplitude of signals within a selected span. You can use it to identify harmonics and spurious signals, examine the noise floor, and evaluate signal quality. Each reading depends on the settings, so write down the span, RBW, and attenuation with the result.

Dynamic range describes the difference in level between the strongest and weakest signals an analyzer can measure simultaneously. The available dynamic range depends on the model and its specifications. For a component's frequency response with phase, you need a vector network analyzer.

How Do You Use a Spectrum Analyzer? Step-by-Step Guide

These 7 steps walk you through setting up a spectrum analyzer and interpreting the results. Start with the 4 settings that have the greatest impact on your measurements.

Setting What it does Trade-off
Span Sets the start-to-stop frequency range A wide span shows more but with less detail
RBW Sets the IF filter width A narrow RBW separates close signals and lowers the displayed noise, but slows the sweep
Reference level Sets the level at the top of the display Set it so the largest expected signal fits on screen
Input attenuation Reduces the level at the input mixer More attenuation helps prevent distortion but raises the displayed noise floor
Setting
What it does
Trade-off
Span
Title
Sets the start-to-stop frequency range
Title
A wide span shows more but with less detail
RBW
Title
Sets the IF filter width
Title
A narrow RBW separates close signals and lowers the displayed noise, but slows the sweep
Reference level
Title
Sets the level at the top of the display
Title
Set it so the largest expected signal fits on screen
Input attenuation
Title
Reduces the level at the input mixer
Title
More attenuation helps prevent distortion but raises the displayed noise floor

1. Connect the Signal

  • Use a cable rated for the range: Connect the signal source to the RF input using a coaxial cable rated for the frequencies you are measuring.
  • Respect the input limit: Never exceed the maximum input level on the data sheet.

2. Set the Frequency Range

  • Know the expected frequency: This guides the start and stop frequencies, or a center frequency and span. The span is the difference between start and stop.
  • Start wide, then narrow: A wide span helps you locate signals across the frequency range, while a narrower span lets you examine individual peaks in more detail.

3. Adjust the Resolution Bandwidth (RBW)

  • Understand RBW: Resolution bandwidth is the width of the IF filter. A narrower RBW separates closely spaced signals and lowers the displayed noise floor, but slows the sweep.
  • Match the RBW to the task: Use a narrow RBW for close signals and a wide one for a quick overview. Thermal noise power is proportional to bandwidth, so doubling the RBW generally raises the displayed noise floor by approximately 3 dB. A University of British Columbia course note explains how an RBW that is too wide can prevent the analyzer from distinguishing closely spaced signals and increase the noise included in the measurement.
Two stacked spectrum plots of the same two close signals, marked by dashed lines at their two frequencies: with a wide RBW they merge into a single peak, and with a narrow RBW they show as two separate peaks over a lower noise floor
A narrower RBW separates two close signals that a wider RBW merges into one peak, and it lowers the displayed noise floor. Source: Keysight illustration. | spec: two stacked line plots of amplitude against frequency, same frequency axis, no numeric values. Top plot labeled "wide RBW": one broad peak. Bottom plot labeled "narrow RBW": two distinct narrower peaks at the same two frequencies. Top plot baseline visibly higher than bottom (wider RBW raises the displayed noise floor). Units: none (conceptual). Data source: the resolution bandwidth behavior described in Keysight's What Is Resolution Bandwidth? glossary entry.

4. Set the Reference Level and Attenuation

  • Reference level: Sets the level at the top of the display. Adjust it so the largest expected signal fits on the screen.
  • Attenuation: Reducing the signal amplitude can prevent distortion and saturation. Set it by hand or use the automatic setting if your analyzer has one. A 2020 Keysight blog describes the input mixer level as a trade-off between distortion performance and noise sensitivity.

5. Analyze the Signal

  • Read the peaks: Start with the expected signal. Peaks indicate energy at particular frequencies.
  • Find the noise floor: Look at the baseline between signal peaks to estimate the displayed noise floor. Record the RBW with your measurement.
  • Use markers: Place a marker on a peak to read its frequency and amplitude.
  • Compare with what you expect: An unexpected peak or level can point to distortion, interference, or a setup error.

6. Apply Advanced Analysis (Optional)

  • Harmonics and spurious signals: Harmonics appear at integer multiples of the fundamental. Keysight's EMI testing page describes using a signal analyzer or EMI receiver to troubleshoot and identify suspected disturbances.
  • Noise measurement: Examine a frequency range without expected signals. Record the RBW so the noise reading can be interpreted correctly.
  • Demodulation: Some analyzers can demodulate modulated signals to analyze their content.

7. Save and Review the Results

  • Capture the display: Save the trace as an image or data file for documentation or review.
  • Annotate your results: Label key features so they are easy to recall.
  • Review the data: Check whether the results match your expectations and note any measurements that need further investigation.

Accuracy depends on the instrument model and its calibration, so read the data sheet for the figures that matter to your measurement.

Frequently Asked Questions

A spectrum analyzer measures the amplitude of a signal at each frequency across a chosen span. That shows the signal's frequency components, including harmonics and noise.

An oscilloscope shows a signal's amplitude against time. A spectrum analyzer shows amplitude against frequency.

A spectrum analyzer measures an existing signal and typically has no built-in source. A vector network analyzer (VNA) supplies its own stimulus and reports amplitude and phase, so it shows how a component responds.

Resolution bandwidth (RBW) is the width of the IF filter. A narrower RBW separates closely spaced signals and lowers the displayed noise floor, but slows the sweep.

Need Tech Support?

Not sure which model fits your application? Talk to our technical support team and they will help you choose.

Browse Used Spectrum and Signal Analyzers

Keysight Premium Used test equipment
Keysight Premium Used test equipment offers like-new Keysight performance at a fraction of the cost. Source: Keysight.

Start with the highest frequency you need to measure, then compare the noise floor and installed options in each data sheet before you pick a model.

Spectrum Analyzersの特価製品

すべてを見る Spectrum Analyzers
  • Like-new Condition
  • Updated Firmware
  • Full Calibration
  • New Accessories
  • Like-new Warranty
  • Customization possible

Learn more

  • Savings of up to 90%
  • Working Condition
  • Calibrated or Tested
  • 30-Day Right-of-Return
  • No Customization
  • Shipping to limited countries

Learn more

Select up to 3 instruments to compare

Cancel
Select another instrument to compare
Starting at
Select another instrument to compare
Starting at
Select another instrument to compare
Starting at

Whenever You’re Ready, Here Are
5 Ways We Can Help You

2

Call tech support US: +1 800 829-4444
Press #, then 2. Hours: 7am – 5pm MT, Mon– Fri

3

Contact our sales support team

4

Create an account to get price alerts and access to exclusive waitlists

5

Talk to your account manager about your specific needs

Sources

Callum Reed
Used Equipment Store Marketing Manager
ご意見・ご感想をお寄せください
Stay Up to Date on Used Equipment!

Don’t miss special offers, news, and announcements on the latest used equipment. Unsubscribe at any time.

Get Email Updates