The DS1321A High Precision Fault Injection Probe Tips can increase fault injection success rates by creating precise, local glitches in modern chips.

Highlights

High Precision Fault Injection Probe Tips can provide a precise, local glitch using powerful electric magnetic pulses. Our unique production technique results in high precision tips featuring small coils, which produce a local glitch that, with multiple windings, still delivers enough power to drive successful fault injection attempts. Due to our smaller coils, the penetration depth of our High Precision Fault Injection Probe Tips is lower compared to larger probe tips, so that preparing, or decapping, the chip may be necessary.

  • Reduces the area of impact for the injected fault, making it easier to analyze exactly which part of the chip is vulnerable
  • Increases fault injection success rate
  • Due to the tips’ high power, decapping a chip is not always required

역량확대

다른 도움이 필요하십니까?