Bandwidth Boosting Techniques for the Infiniimax Probe Amp and Probe Head
Show Description
Keysight InfiniiMax differential probes are DSP corrected to have a flat magnitude and phase response to provide the highest possible accuracy. The bandwidth chosen to correct to is typically around 3dB non-corrected bandwidth. Usually, extending the bandwidth much beyond that point will increase the noise floor, and if pushed even further, can cause unrealistic noise artifacts. This application note presents the techniques used to extend the bandwidth performance of the InfiniiMax 1169A/B and the N5381A/B solder-in head using the PrecisionProbe application on Infiniium realtime oscilloscope.