Increasing Throughput on the In-Circuit Test (ICT) System

アプリケーションノート

Why does test time increase?

 

Firstly, know that longer test times can arise due to various reasons:

– The test generated from the Interactive Program Generator (IPG) may not be optimized for the specific production board revision

– Addition of test options when debugging tests the first time

– Addition of test options during production testing

– Incorrect interrupt analog test

– Incorrect power up

– Using default vector cycle to test digital devices

– Overly long wait during powered test

– Using “safeguard cool” command arbitrarily

– Overly complex test

– Immoderate wait in “testplan” file

– Incorrect GP-Relay usage

– Poorly maintained i3070 system hardware