White Papers
Part 3: MIMO and Beamforming
Multiple-input / multiple-output (MIMO), beam steering, and beamforming are the most talked about technologies in 5G. They are essential for delivering the 100x data rates and the 1,000x capacity goals the International Mobile Telecommunications-2020 (IMT-2020) vision specifies.
According to the Ericsson Mobility Report 1(June 2019), mobile data traffic grew 82% year on year in the first quarter of 2019. The report predicts mobile traffic will rise at a compound annual growth rate of 30% between 2018 and 2024. It forecasts a total of 8.8 billion mobile subscriptions by 2024, including 1.9 billion for 5G enhanced mobile broadband.
O que você está procurando?