Solutions for WLAN 802.11ac Manufacturing Test

Notas de Aplicação

The number of wireless devices on the market these days is exploding and, as a result, so too has the number of users—many of whom now carry multiple wireless devices (e.g., cell phone, laptop or tablet). More and more, these devices are providing functionality beyond the ability to just make calls or surf the Internet. That trend, along with today’s countless other media-rich applications, is pushing current bandwidth availability to its limit and driving the need for wireless technologies capable of increasing bandwidth capacity. One such technology, 802.11ac, promises to deliver the higher data rates necessary to meet consumers ever increasing data demands. Unlike other standards being rolled out, it achieves this relatively cheaply by leveraging the same 5-GHz technologies that are now well established with 802.11n.