HDMI and DisplayPort Design and Test Solutions

Notas de Aplicação

The High-Definition Multimedia Interface (HDMI) and DisplayPort (DP) interfaces are being implemented broadly in devices from high-definition televisions to personal computers to set-top boxes. The overwhelming concern for developers of these products is interoperability. Interoperability starts with the physical layer where the digital content is driven from one device through media such as a cable to a receiving device. Tools to measure the parameters of these devices are required to understand if the device is in compliance, or how close the device’s performance is to the specification.