Streamlining High-Volume PCB Testing

Notas de Aplicação

High-volume PCB manufacturing demands maximum throughput with minimal floor space and operational overhead. Traditional production lines rely on multiple, disconnected test stations — In-Circuit Test (ICT), programming, and Functional Test — introducing non-value-added “dead time” that increases cycle time and complexity.

 

This application note explores how consolidating these test processes into a single, unified platform using the Keysight i7090 Board Test System streamlines production flow. By eliminating station-to-station transfers and leveraging a massively parallel architecture, manufacturers can reduce cycle time, simplify operations, and keep pace with high-speed SMT lines without expanding their production footprint.