Exhibitor UI Command Injection

Strike ID:
E19-0ul11
CVSS:
9.8 CVSS:3.1/AV:N/AC:L/PR:N/UI:N/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
3
Year:
2019

Description

This strike exploits a command injection vulnerability in the Exhibitor Web UI. The vulnerability is due to improper parsing of parameters passed to the config editor web form. A malicious attacker can exploit this by performing a specially-crafted HTTP request. Successful exploitation leads to arbitrary commands being run in the context of the user running the Exhibitor server.

CVE

References