A quick model QA function during the parameter tuning process.

Highlights

The W6022E PathWave MBP QA Express includes:

  • A one-click model QA function during model parameter tuning
  • Default check rules according to the model types
  • A graphical user interface to review the checking result

The W6022E includes an independent Add-on QA Express to the model extraction tool MBP. QA Express offers a one-click model qualification function during model parameter tuning.

역량확대

다른 도움이 필요하십니까?