The Dynamic Sequencing Option SP2 enhances the “segment advance” ARB capability to allow jumping to any of the 256 different segments in ARB Waveform Memory. The next segment to be played is determined dynamically via an 8-bit value input on pdata(7..0) and is strobed in using the patt_trig_in2 signal.