Emulate Sustained and Evolving Lunar Networks

백서

Most lunar communication systems today rely on dedicated, point-to-point links built for a specific rover, lander, or scientific instrument. That approach works for individual missions, but it will become increasingly difficult to manage as more astronauts, vehicles, habitats, sensors, autonomous systems, and experiments arrive on the Moon. A shared cellular network based on 4G, 5G, and eventually 6G technology could provide a more scalable and interoperable solution.

 

Cellular base stations on the lunar surface could deliver continuous connectivity, support users on the move, provide higher data rates, and simplify network management. Astronauts and robotic vehicles could stay connected as they travel, while scientists could transmit data, control instruments, and oversee autonomous operations from a distance. The same network could connect equipment within and between habitats. Over time, it might also support activities such as monitoring food production, automating water and nutrient delivery, coordinating supply landings, and managing the enormous amount of data generated by a permanent lunar community.

 

Building this network around established 3GPP standards would offer several advantages over creating proprietary communication systems for each mission. Commercial 4G and 5G technologies already include mobility management, beamforming, multiple-input multiple-output antennas, efficient use of spectrum, and mature communications protocols. Existing chipsets and standardized interfaces could reduce development time and risk while providing a clear path toward future 5G and 6G capabilities. Shared standards would also make it easier for new missions, devices, base stations, and international partners to work together.

 

Of course, the Moon is an unforgiving place for wireless technology. Craters, mountains, boulders, and uneven terrain can block radio signals or cause them to reflect and scatter, resulting in multipath propagation, fading, and coverage gaps. Lunar dust creates another challenge. It is sharp, electrically charged, and easily disturbed, allowing it to cling to antennas, spacesuits, mechanical steering systems, and other equipment. Over time, that buildup could affect both signal quality and hardware reliability. Communications equipment must also survive intense radiation, extreme temperature swings, and the Moon’s near-vacuum environment.

 

Many of these risks can be studied on Earth before equipment is ever launched. Engineers can combine computer modeling, channel emulation, and wireless network analysis to create realistic simulations of lunar conditions. LIDAR data collected by lunar orbiters can be loaded into ray-tracing software to reproduce craters, hills, rocks, dust, and other surface features. Researchers can then study how signals are likely to travel between landers, habitats, base stations, rovers, and astronauts in different locations.

 

Keysight’s PROPSIM channel emulator can bring these modeled conditions into the laboratory by applying them to real or simulated communications equipment. In effect, engineers can recreate the Moon’s radio-frequency environment without leaving Earth. They can test 4G, 5G, Wi-Fi, user devices, and base stations under multipath, fast-fading, shadowed, line-of-sight, and non-line-of-sight conditions. Keysight’s WaveJudge wireless analyzer adds another layer of insight by decoding cellular protocol activity and revealing the radio behavior behind changes in throughput, channel quality, and block error rates.

 

As in-phase and quadrature radio data is collected on the lunar surface, engineers can feed those real-world measurements back into their models. This creates an ongoing process in which the network becomes more accurate and capable over time, rather than being designed once and left unchanged. Mission planners could use the updated models to evaluate rover routes, coverage areas, antenna designs, bandwidth requirements, access-point locations, reliability targets, and the connectivity needs of individual experiments. The same approach could help determine where future communications towers and habitat wireless systems should be installed.

 

Ultimately, a successful lunar network will need reliable coverage, enough capacity to carry growing amounts of data, support for users in motion, built-in redundancy, and the flexibility to evolve. By combining cellular standards, lunar base stations, satellite links, realistic simulation, and continuous measurement, space agencies and technology companies can build dependable communications and navigation infrastructure—not only for lunar research and long-term habitation, but also for future exploration deeper into the solar system.