Top 5 Strategies for 5G Component Characterization and Test

백서

5G represents significant revenue potential for the entire mobile ecosystem. That includes chipset and component manufacturers, device makers, network equipment manufacturers, and service providers. 5G is also an exponential increase in technical complexity. Massive multiple input, multiple output (MIMO) antennas, for example, require multiple transmission and reflection measurements for each antenna element.

Component manufacturers need to deploy effective strategies for characterization and test regardless of the component type (amplifiers, mixers, converters, etc.). To win the 5G race, component manufacturers need greater confidence across the workflow. Measurement integrity is essential to gain deeper insights into designs in research and development (R&D). Component manufacturers also need to accelerate time to market and reduce test costs to stay competitive. The high throughput of true multiport test setups gives component manufacturers the performance they need to keep up with aggressive timelines.