Journey Of A Signal

백서

The Journey of a Signal: Optimize Your Signal Analysis Measurements explains how a signal analyzer processes a device under test (DUT) signal and why analyzer setup choices can affect measurement accuracy. The white paper is written for engineers who want to understand what happens after a signal enters a signal analyzer instead of treating the instrument as a black box. By following the signal path from input to display, the paper shows how front-end scaling, filtering, mixing, digital conversion, resolution bandwidth, and detector settings influence sensitivity, distortion, noise floor, frequency resolution, sweep speed, and displayed results.

 

The paper begins with the RF input attenuator and pre-amplifier. When a DUT connects to a signal analyzer input, these components scale the signal to levels the rest of the analyzer can process. The attenuator and pre-amp also help control the signal level shown on the display and influence signal-to-noise ratio (SNR). For low-level signals, reducing input attenuation and enabling the pre-amp can improve sensitivity, formally described as displayed average noise level (DANL). For high-power signals, adding attenuation can help prevent overload, distortion, and gain compression. This section helps engineers understand how analyzer settings can either reveal or mask DUT behavior.

 

The asset then follows the signal through filtering and mixing. In entry-level spectrum analyzers, the signal typically passes through a bandpass filter. In analyzers with a pre-selector, a tunable bandpass filter sweeps across the frequency domain and determines which frequency range the analyzer acquires at a given time. The paper then explains the mixer, a three-port nonlinear device that combines the DUT signal with a local oscillator (LO) signal. The mixer output includes the sum and difference of the input and LO frequencies. When the mixed output equals the intermediate frequency (IF), it passes through the IF filter for downstream analysis. The paper also notes that mixers can add spurs, noise, or harmonics, so engineers must distinguish true DUT characteristics from analyzer-introduced artifacts.

 

The white paper explains how digital signal processing affects the measurement. After the signal is mixed and converted from analog to digital, it passes through the IF filter. The key user-controlled setting in the IF filter is resolution bandwidth (RBW), which determines the minimum separation required for two frequency components to appear as separate signals on the analyzer screen. A wide RBW supports faster sweeps but raises the noise floor and reduces horizontal resolution. A narrow RBW takes longer to sweep but provides better frequency resolution, lowers the noise floor, and supports detailed analysis of spurs or closely spaced signals. This section gives engineers a practical framework for choosing RBW based on measurement objective rather than default behavior.

 

The asset also explains digital detectors. Because the analog-to-digital converter captures more data than the display can show, digital detectors select representative data points from bins using different algorithms. Detector selection affects whether the display emphasizes maximum values, minimum values, averages, extremes, or signal stability. Understanding this behavior helps engineers make more defensible choices when evaluating peaks, noise-like signals, and measurement repeatability.

 

Overall, this white paper provides a concise but practical guide to signal analyzer operation and setup optimization. It is relevant for RF testing, education, device characterization, troubleshooting, signal validation, and general-purpose signal analysis workflows. Engineers can use it to understand how analyzer configuration affects measurement results, reduce false readings, and improve confidence when interpreting signals that pass through attenuation, amplification, filtering, mixing, digitization, and detection stages.