5G Evolution. Revolution. Reality.

전단지

5G Evolution. Revolution. Reality.

Enabling Transformative Research  

As the leading provider of test and measurement solutions for wideband RF, microwave and millimeter-wave technologies, we have two primary goals in 5G. One is to assist commercial researchers as they accelerate the development and verification of new-generation designs. The other is to help researchers in academia explore groundbreaking concepts with greater precision and deeper confidence. We’re supporting these efforts with an unmatched range of 5G solutions based on Keysight hardware and software products. All will assist engineers and scientists as they drive the evolution of existing technologies, create revolution through new innovations, and transform the vision of 5G into reality.

Helping Create the Standard and Fostering Research Partnerships  

The race is on to demonstrate successful implementations of 5G. Keysight has been there from the beginning, collaborating with the earliest players in 5G and supporting advanced research and experimentation. One conduit is Keysight Laboratories, which is our central resource for applied research. Laboratories staff has been, and continues to be, engaged with numerous commercial customers as well as the relevant consortia and standards bodies. Another important link is Keysight University Relations, which sponsors and mentors university research. This level of direct involvement provides a firsthand view of the latest technological and marketplace developments. From that vantage point, we’re offering measurement insight as the industry defines next-generation standards and the necessary test procedures. We’re also applying that knowledge to the creation of new-generation instrumentation and software that provides headroom to meet current and evolving challenges.