백서
The global automotive DC-DC converter market is expected to be 18.7 billion by 2028 with a compound annual growth rate of 10% from 2023-2028.
DC-DC converters are an essential part of the vehicle, converting voltages to power various onboard systems, such as increasingly sophisticated infotainment, and enhanced safety features using advanced driver assistance systems (ADAS).
The growing adoption of electric vehicles (EVs), both battery-powered and hybrid EVs (HEVs), is also boosting the demand for DC-DC converters.
Let’s examine some of the industry trends and technology that are helping to support the development of more efficient DC-DC converters.
무엇을 찾고 있습니까?