Increasing Electronic Device Power Efficiency

백서

Increasing Electronic Device Power Efficiency Through Proper Testing

To be competitive in today’s consumer electronics industry, manufacturers must constantly innovate on the design of their devices, especially as consumers demand devices that are smaller with more features, faster speeds, and longer run times. However, as devices shrink, power challenges grow. Batteries, external power source, or some combination of the two power all electronic devices from mobile phones to toys to medical devices. Additionally, electronic devices often contain several sub-circuits that each has a voltage level bias requirement that differs from the voltage level supplied by the battery or external power source.