애플리케이션 노트
Computing technology and the Internet have dramatically change our lives and the boom of new technology, the Internet of Things (IoT), continues to expand the range of Internet connected devices including wearable devices, sensors, wireless networks, home appliances, electric vehicles and so on. These new devices and applications require long life operations with low signals and limited power supplies from batteries or other harvested energy supplies. With this ever-expanding range of devices comes an increasing demand in the need to analyze the current profile for research, development and the debugging of low power devices and circuits. A current probe with an oscilloscope has been commonly used for measuring such dynamic current behavior. However, it is becoming difficult to measure the low current of μA or less flowing in the next generation low power devices.
무엇을 찾고 있습니까?