TS-8989 System Integration Guide

애플리케이션 노트

In today’s manufacturing environment, floor space is an increasingly invaluable variable in the cost of test equation. One way to optimize space is to do more with the existing workstations and rack space. Keysight’s TS-8989 PXI functional test system is designed as an integrated all-in-one measurement and high current switching box solution, providing flexibility for manufacturers to optimize the latter. In this application note, an example of integrating the TS-8989 in a typical rack is shown as a guidance on key considerations when determining rack type, power distribution, mass interconnect and cabling. Figure 1a shows the front view for instrumentation connectivity, and rear view for DUT connectivity. Figure 1b shows the side view of the TS-8989 system with dimension in millimeters for user reference when designing custom structures to enclose the system.