동영상
How do you test Wi-Fi and 5G network equipment and devices? The answer is with the innovative Octobox testbed.
Understand how the Octobox testbed tests Wi-Fi and 5G network equipment and devices by simulating real world environments such as interference, traffic, and mesh handover in a stable, automated, and repeatable testing environment. With the advent of Wi-Fi 6, 6E, and now Wi-Fi 7, comprehensive testing is more vital than ever.
Our vendor-neutral approach accelerates your validation activities and provides the ability to compare and certify vendors, while optimizing costs and performance. The Octobox system supports IEEE 802.11 and the Broadband Forum TR-398 performance standards, and with the addition of Octobox automation test packages you can accelerate your testing with standards-based test plans.
By identifying potential problems early in the development cycle, Keysight’s OCTOBOX configurable testbeds can help you ensure your devices and networks are prepared to meet the demanding wireless future.In a world driven by connectivity, end users are demanding reliable, robust network services and devices. If bugs or breakdowns in the network are discovered after launch, service providers, device manufacturers, and network vendors can spend millions in troubleshooting, customer care costs, and efforts to repair damaged reputations. And with the advent of Wi-Fi 6, 6E, and 7, testing is more vital than ever.
Keysight Octobox wireless testbeds ensure your networks and devices will be prepared to meet the demanding wireless future. By identifying problems early in the development cycle, we can help deliver a flawless experience to your customers. Our highly realistic test suites recreate real world conditions, allowing you to evaluate the performance of the latest Wi-Fi and 5G network equipment and devices.
무엇을 찾고 있습니까?