Vision X 400G (Model: Vision X 400G) Network Packet Broker

데이터 시트

Keysight’s Vision X is the next-generation network visibility solution. It delivers expandability and flexibility that meets the ever-evolving needs of the data center. Vision X is a high-density, modular chassis comprised of customizable front modules and multi-speed port choices. It also supports a rear, advanced packet processing module, extending the total packet processing capacity of the chassis.

 

Vision X is now getting even better with a new and field upgradable Vision X 400G switch card, extending visibility coverage from 10G all the way to 400G. All existing modules will continue working as-is after the 400G switch card upgrade. Your past investment is fully protected with the upgrade.